STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Can't connect to ST-Link with CLI

Hi there,I have an ST-Link V2 which i want to use for programming a .bin file to an stm32G0 MCU. Afterwards i want to set the RTC register to the time beeing. It already works "manually" but i wanted to write a script to automate the process.I alread...

vs_rzb by Associate II
  • 2295 Views
  • 3 replies
  • 1 kudos

Resolved! No STM32 target found - STM32G030K6T6

Hi, I'm making a board for UART and I2C communication.Please refer to the schematic below;  I put 5V External power supply at VBUS,and connects SWDIO, SWCLK, NRST, 3V3, GND to the STLINK V3 Minie. However it shows "No STM32 target found" message on S...

SungjaeKim_0-1737011644144.png

STM32F070F6 bootloader

STM32 cube programmer doesn't recognize my custom board neither via USB DFU nor USART.My circuit is simply the STM32F070F6, a 12 MHz crystal and some LEDs to control (also caps and res as necessary).Even with boot0 direct in high or low, I'm not able...

EdDn by Associate
  • 2151 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.