STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! CubeProgrammer API examples not working

I've just compiled the USB_Example.cpp example and its reporting an initialization error on running (The application could not initialize correctly (0xc000007b)), I have VS 2022 fully updated, I did not migrate the project to the latest toolset to av...

Robmar by Senior III
  • 8313 Views
  • 25 replies
  • 4 kudos

CubeProgrammer - DFU Error?

I have a custom board with an STM32H747XI with BOOT0 tied to 0. I want to jump to the bootloader from my application so that I can perform a USB DFU. The USB works correctly. I have a terminal app that I use to connect to the VCP. If I send a specifi...

C-Coder by Associate III
  • 2271 Views
  • 4 replies
  • 1 kudos

Stop SWV

Hi,I am launching Serial wire viewer from external application.The below  command allows the user to access the serial wire viewer console mode,which displays the printf data sent from the target through SWO.STM32_Programmer_CLI.exe -c port=swd SN=37...

Shimjith by Associate
  • 1020 Views
  • 1 replies
  • 1 kudos

Resolved! Secure Firmware Install over USB on STM32H743

Is it possible to securely install firmware over USB on the STM32H743?  I am getting the error below when trying to download my SFI file.  MCU has been powered up with BOOT_0 pin high.  STM32CubeProgrammer finds and connects correctly to chip. 11:03:...

scottro by Associate II
  • 2190 Views
  • 3 replies
  • 0 kudos

STM32CubeProgrammer v2.19 released

We are pleased to announce that STM32CubeProgrammer 2.19 is available What is new in 2.19: Support for the STM32WBA6xxx microcontrollers: Internal memory programmingOption byte/OTP programmingRDP regression with passwordSFI support Support for MCE N...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.