2024-02-08 2:44 PM
Hi there, I am hoping this forum will be able to help me:
This is my first time using the STM32 Nucleo-64 board (STM32F303RET6) as well as the external ST-LINK/V2 programmer. I just wrote a simple program that turns on the LED but I am having trouble connecting to the board. I am almost positive I have correctly wired the two together (using GND, VDD (3.3V), SWDIO, and SWCLK). I have reinstalled the correct drivers and updated the software. I've tried a few different ways of connecting using recommendations from other forums. These are the errors I've been getting:
From stm32cubeIDE:
From stm32cubeProgrammer:
From stm32 st-link utility:
I've tried different frequencies and modes but I still get the same errors.
Weirdly, when I try to connect to the target through the utility application, the st-link lights up green and the stm32 board starts flashing (even though it says it can't connect). Is this normal?
I just need to know how to successfully connect to the board so I can flash my program. Any advice would be appreciated!
2024-02-08 3:46 PM
The nucleo board has an onboard st-link. You don't need an external programmer for it. Just need to connect CN1 with a USB cable to your PC.
2024-02-08 4:50 PM
Connecting what to what? The Nucleo is hard wired.
Check the jumpers for SWDIO / SWCLK connect to the local target.
Then perhaps ponder why the voltage isn't reading 3 - 3.3V
2025-05-06 10:14 PM
Did you manage to solve this issue? I faced the same problem while working with UART
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.