STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Download .hex & .bin onto STM32F100C8-Doesn't Work

Hi,I am currently using the following microcontroller (STM32F100C8T6B) in my design. I have built my project using the STM32CubeIDE (STM32CubeIDE Version: 1.18.1). I have created the following output files (BIN, HEX, and ELF) and I was able to RUN an...

WJ1 by Associate II
  • 1658 Views
  • 2 replies
  • 3 kudos

Resolved! STM32 BOOT0 not working

I have designed a board using the STM32U083KCU, i have programmed it once with a simple program made with STM32CubeIde that only prints "Hello\n" over USART2 on pins PA2 and PA3. I have flashed the chip over the same pins by holding the BOOT0 Pin hig...

Polonez by Associate II
  • 2612 Views
  • 5 replies
  • 3 kudos

Resolved! Even I a customer!

Well, that's the strangest 'support' department I've ever dealt with.In trying to download the STM32CubeProgragger for Linux, I've found that the download halts at ~40Mb of some 280MB, or so. Tried downloading as user, and as guest, no luck. Tried di...

M_de_Luis by Associate II
  • 5544 Views
  • 11 replies
  • 4 kudos

Resolved! External Loader

Hello all,I have a custom board with an STM32U5A9 mcu with an external MT25QL128 flash for TouchGFX assets.I have a working loader for IAR Embedded workbench and I'm trying to port it to work with the STM32CubeProgrammer.When building as a normal pro...

RW3562 by Associate II
  • 2494 Views
  • 6 replies
  • 1 kudos

Making the DTR/RTS option support CH340

Almost all development boards produced by Chinese vendors use CH340 as the uart converter chip, I would like stm32cubeprogrammer to be able to control the RTS and DTR of this chip.If the feature works fine for the FT232RL, I don't know why it won't w...

wc7086 by Associate II
  • 8056 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.