2025-05-12 5:03 AM - edited 2025-05-13 12:57 AM
Hello everyone,
I am currently writing a GUI application with QT. The STM32CubeProgrammer API is integrated in the project. So far I was able to flash FW, use functions like massErase and execute without any problems (All these over UART). Now my MCU needs the nBOOT0 option bytes to boot correctly.
I have tried several times with the STMCubeProgrammer API function "sendOptionBytesCmd" but it does not work. I always get a "-6" as return value. Does anyone have an idea how to solve this ?
This is what my code looks like.
qDebug() << "Setting Option Byte nBOOT0 to 1";
int sendOptionBytesCmdFlag = sendOptionBytesCmd((char*)"-ob nBOOT0=1");
if (sendOptionBytesCmdFlag ! = 0) {
disconnect();
qDebug() << "Could not set Option Byte nBOOT0 to 1";
}
qDebug() << "Option Byte nBOOT0 set to 1 successfully! " << sendOptionBytesCmdFlag;Thanks in advance :)
2025-05-16 7:05 AM
Hello @csmk59,
I have added your code into the UART example on QT API project with an STM32G474 and it works well on my end. Could you provide more information about your setup? exact part number of your STM32G4? CubePorgrammer version and any additional details (logs, UART configuration...).
Thanks,
Amine.
2025-06-03 6:53 AM
Hello @csmk59,
Any feedback?
Thanks,
Amine.
2025-06-05 1:43 AM - edited 2025-06-05 1:54 AM
Hi @Amine_Jridi
Sorry for the late reply.
The exact name of my MCU is “STM32G431CBY3TR.”.
I even have the latest version of the STMCube32 Programmer API. That didn't work either.
There aren't many log files. As I said, everything works except for setting option bytes. Sometimes I get -1 as the return value or even -6. I don't understand.
This is how the UART connection was established.
usartConnectParameters port{"", 115200, EVEN, 8, 1.0f, OFF, 0, 0, 0, 0, 0};As I said before, Firmware download, chip erase, everything works perfectly.
Regards,
Claude
2025-06-24 6:20 AM - edited 2025-06-24 6:21 AM
Hello @csmk59,
I have attempted to reproduce the issue you described, but everything is functioning correctly on my side.
To help you better understand the error codes, please refer to the API documentation available at:
> /Path/To/CubeProgrammer/API/doc
In particular, the return value -6 corresponds to CUBEPROGRAMMER_ERROR_INTERFACE_NOT_SUPPORTED, which means that the interface is either not supported or not implemented on this platform.
Thank you,
Amine
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.