2020-08-23 10:44 AM
Hi have a simpler STM32 application which includes below simpler code in main.c file.
#include <stdio.h>
int main(){
int a=10, b=20;
printf("Sum=%d \n", a+b);
return 0;
}Later i build the project in RELEASE mode and ran the application then it was throwing below error.
STMicroelectronics ST-LINK GDB server. Version 5.6.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0-RC1
-------------------------------------------------------------------
ST-LINK SN : 066DFF535254887767171939
ST-LINK FW : V2J37M26
Board : 32F469IDISCOVERY
Voltage : 3.27V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x434
Revision ID : Rev A
Device name : STM32F469xx/F467xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a02796.srec
File : ST-LINK_GDB_server_a02796.srec
Size : 4920 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.382
Verifying ...
Download verified successfully
Debugger connection lost.
Shutting down...
Can anybody help me in resolving this issue?
Thanks,
Hari
2020-08-23 11:30 AM
> below error.
What error? The program says it was downloaded and successfully verified.
Also, never return from main().
2020-08-23 10:38 PM
Hi @TDK ,
I am new to micro-controller programming. Also, I'm not sure why i'm seeing "Debugger connection lost.Shutting down..." at the end.
It would be very helpful if you respond with some explaination/resource.
Also I'm not seeing printf output anywhere in the console. This is the reason I'm feeling Runtime it was not working. How can i see the printf() output.
2020-08-24 6:58 AM
Not real sure. Your question essentially boils down to something not working with little to no additional info. Hard to debug that remotely.
There is no standard way for printf to behave. Some people port it to UART. Some to SWO output. I don't know which configuration you're using.
Where are you getting this example? Have you looked at and ran STM32CubeIDE board examples?
2020-08-24 7:14 AM
Hi @TDK ,
Please let me know, What additional iinformation you required to understand this problem.
This is very simpler example to add two numbers.
I have not taken a look at STM32CUBDEIDE examples.
2020-10-06 10:59 PM
STM32CubeProgrammer v2.5.0-RC1
V2.5.0 doesn't support for STM32F4 . for this please check the STM32CubeProgrammer document .
So, download the STMCube IDE (v 1.1.0 )
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
Log output file: C:\Users\Techno\AppData\Local\Temp\STM32CubeProgrammer_a17472.log
ST-LINK SN : 0669FF545052836687104442
ST-LINK FW : V2J37M26
Voltage : 2.88V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x419
Device name : STM32F42xxx/F43xxx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a17472.srec
File : ST-LINK_GDB_server_a17472.srec
Size : 48836 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 2]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.669
Verifying ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.