STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

How do I install this on Mac Big Sur 11.4 ?

I download the package onto my Mac in the Download folder.I open a terminal and navigate to the Download/en folder.I execute the command "./SetupSTM32CubeProgrammer-2.7.0.app/Contents/MacOs/SetupSTM32CubeProgrammer-2_7_0_maco"I receive a popup window...

LHarm.1 by Associate III
  • 1091 Views
  • 2 replies
  • 0 kudos

Hello everyone. How to passthrough a device STM32F05x to a VM in VMWare Horizon (Client-Agent via USB Redirection)?

On the host the card is connected correctly and is being seen by STM32CubeProgrammer (v.2.6.0). On VM upon connection it recieves just the same drivers (the same ID etc), but Programmer doesn't see it at all. It is still somehow available by Putty, b...

I have downloaded and installed STMCubeIDE 1.6.1 and using it along with ST-Link/v2-Isol JTAG programmer .How can i import, debug and flash the (.elf) file which is generated from any external source say Jenkins?

I need to be able to import the .elf file into my STMCubeIDE and perform debugging and run the code. The (.elf) file is generated in Jenkins through nightly builds. Can i know the procedure for this?

AJali.1 by Associate
  • 1379 Views
  • 1 replies
  • 0 kudos

Resolved! STM32 Cube programmer firmware read problem

Hi All, Until now with F3 and F0 devices we were able to upload and download firmware files to and from MCUs using "BootloaderDemo" application from STM. That software had both upload and download capabilites. With the newer G474 device however, we h...

ma.alam9 by Associate III
  • 5026 Views
  • 4 replies
  • 0 kudos

Resolved! cannot execute binary file: Exec format error

I made a NUCLEO-G474RE IO-Toggle project in eclipse on Ubuntu, the building has been passed through, while I couldn't run it into the NUCLEO board. When I start to debug it, this error was shown:/bin/bash: /home/mq/eclipse-workspace/test_NUCLEO-G474R...

0693W00000Bd0IlQAJ.png 0693W00000Bd0IqQAJ.png
MQi.1 by Senior II
  • 30372 Views
  • 2 replies
  • 0 kudos

STM32H7 Hard Fault

I have a program where data is read into the dataStore buffer of a double buffered system from external flash memory via SPI upon detection of an interrupt, around every 700ms; the only ISR sets a value and if the block in my main loop detects this v...

NSR by Associate III
  • 8493 Views
  • 5 replies
  • 0 kudos

Resolved! CubeProgrammer_API not setting verbosity level

I have managed to use the CubeProgrammer_API.dll in a visual studio C# project. Everything seems to be working properly but when I try to set the verbosity level nothing changes. It seems to be fixed to level 2. This is the code I'm using:[DllImport(...

iduque by Associate
  • 1790 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.