STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Hello !!! Some strange error occured when I've tried to transfer a block data. First, Ithe processor received (by serial-DMA) 2006 bytes each time and this is repeated for 240 times resulting an array of 480,000 bytes

The processor is the STM32L4R5 and the SMT32CubeIDE versin 1.6. uint16_t US_Cksum,Trans_Pointer,USA_Data[2006],US_Trans[480000];uint32_t US_Pointer; US_Pointer is zeroed at the start of the program US_Cksum=0;// For Checksu...

INaka.1 by Associate III
  • 5350 Views
  • 14 replies
  • 0 kudos

Custom STM32 Programmer

Hello friends!I have self-developed a programmer for STM32.It works very well.However now I want it to be able to debug in IAR like STLink.Please give me documentation or instructions on how to do it.

Resolved! STM32CubeIDE vs STM32CubeProgrammer

Hi community,I have just started with STM32 MCUs .What is the difference between STM32CubeIDE and STM32CubeProgrammer? I have already installed the STM32CubeIDE and I am able to program the NUCLEO-F030R8 dev. board that I use. So what is the usage of...

Can someone share the commands (CLI) to establish connection once (-c) and do all flash steps, finally disconnect

We are trying to execute the following steps,"C:/Program Files/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32_Programmer_CLI" -c port=SWD --erase all "C:/Program Files/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin/STM32_Programmer_...

PS.7 by Associate
  • 1363 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.