2026-03-30 7:29 AM - last edited on 2026-04-15 8:02 AM by Sara BEN HADJ YAHYA
Finally was able to test STM32CubeMX2 with a NUCLEO-C562RE board.
Simple LED blinking project, and here's what I found out.
Project bloat:
STM32CubeMX2: 26.2 MB of generated data and when compiled 41.1 MB (NUCLEO-C562RE)
STM32CubeMX: 4.6 MB generated and compiled 15.7 MB (NUCLEO-C031C6, same functionality)
The old STM32CubeMX included only the HAL libraries actually used.
The new one dumps everything in.
That's a 5.7x increase for a blink LED.
Missing Release configuration:
Generated CMake project contains only Debug configuration - No Release.
Interesting, because the official "MOOC STM32CubeMX2" video at 4:53 clearly shows both configurations.
Either something changed or the video is misleading.
Creating Release configuration manually requires editing multiple CMake files, including inside the cmake folder — supposedly overwritten on regeneration (in practice, changed only at project creation).
Not trivial if you're not a CMake expert.
I did it once manually, but then ended up using Claude Code AI to do it quickly again.
Linker files buried deep:
The .ld linker files are now hidden under several directory layers (previously at project root).
If you need separate linker configurations for Debug and Release — different memory layouts, for instance — good luck doing that without solid CMake knowledge.
Again, I had to ask AI for help. It's doable, but shouldn't be this complicated.
Bottom line:
The tools work.
If you don't have some CMake experience, will add extra friction.
But basic tasks like Release builds and linker customization shouldn't require AI assistance.
The new interface is fine, just needs getting used to — many settings have moved around.
But a designer tool should better handle these common workflows, not make them this complicated.
Suggestions:
Generate both Debug and Release configurations by default
Include only required HAL driver files
Make linker file customization more accessible
Solved! Go to Solution.
2026-03-30 7:25 PM
You don't compare STM32C031 to C56, do you? STM32C56 is a CM33, with trustzone and lot of components. C0 is a small CM0+.
2026-03-31 1:45 AM
I was not trying to compare head-to-head the run-time performance of these 2 MCUs.
I selected 2 families that could be configured with MX1 and MX2 (and I have both NUCLEO boards).
In MX2 you currently have only the STM32C5 family available, all the rest is in MX1.
I also wanted to select a family without TrustZone, since also STM32C5 does NOT have TrustZone!
Maybe I could have selected the STM32H5 for comparison, it's Cortex-M33 but with TrustZone.
Comparing STM32C5 to another family would not change much regarding the 3 observations in my post.
2026-04-07 2:40 AM
Hello @KPort
We hear you on the Release configuration issue. That's being fixed in an upcoming update. You'll be able to choose Debug, Release, or both when generating your project.
Your points on HAL bloat and linker file accessibility are on our radar too. We're working to optimize these areas and make them less friction-heavy. On family support—for now, new chip families will be added to CubeMX2 going forward, while existing families remain supported in CubeMX.
We appreciate the constructive suggestions and will keep you posted on improvements.
2026-04-08 7:26 AM
Hi @KPort
As a complement to @MorkBeck 's reply, I’d like to confirm that we have an internal tracker open for the topic you raised: missing Release configuration.
Internal ticket numbers: CDM0061318.
I will keep you posted on its progress and on any updates that make it into upcoming releases.
Thank you again for your valuable feedback.
Sara.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.