2025-08-08 1:57 AM
We develop firmware on STM32H7R3L8HxH.
STM32CubeIDE version is 1.19.0
MxCube version is 6.15.0
The problem is that code generator creates additional wrong include file for "regular" H7 MCUs:
#include "stm32h7rsxx_hal.h"
#include "stm32h7xx_hal.h"As this second file does not exist, compiler gives error:
fatal error: stm32h7xx_hal.h: No such file or directoryIn application project it appears in main.h
In bootloader project the issue does not appear, but there is a blank line instead.
In extmemloader project it appears in extmemloader_init.h
Had same problem already STM32CubeIDE v1.18 and we have been manually fixing it (by removing bad include) so far, but it appears that it won't get fixed by itself so I report the issue now.
Solved! Go to Solution.
2025-08-08 3:22 AM
Using your .ioc file, i'm able to reproduce it. I've escalated for correction on the future (under internal ticket number 215537). Thank you so much for reporting this behavior.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-08 2:08 AM
Hello @mkrk
I'm not able to reproduce this on my side (using the STM32CubeIDE version is 1.19.0 and the STM32CubeMX version is 6.15.0). Could you please send your .ioc file for more details.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-08 2:40 AM
Hello @STTwo-32 , here is an obfuscated version of it. I tried creating new project out of it and see the same problem.
2025-08-08 3:22 AM
Using your .ioc file, i'm able to reproduce it. I've escalated for correction on the future (under internal ticket number 215537). Thank you so much for reporting this behavior.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-08-08 3:23 AM
Thanks @STTwo-32 !
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.