2019-02-07 9:48 PM
Using MX 5.0.1 and create a new project "PrjA" for STboard STNM32F401 Nucleo. No changes or configs. Then generate code and open in TrueStudio. Compilation fails because of:
..\Drivers\CMSIS\DSP_Lib\Source\FilteringFunctions\arm_fir_decimate_init_q15.c:41:22: fatal error: arm_math.h: No such file or directory
But the arm_math.h is existing in the folder C:\STM32\PrjA\Drivers\CMSIS\Include.
Is that normal that I have to add a library path to a MX generated project to compile without error?
Then I try to add this path to the project / properties / Includes or Library Paths and get even worse compilation error missing include files.
2019-02-07 10:23 PM
Up's choosing the correct Toolchain/IDE "TrueSTUDIO" help's a lot. Compilation is now OK.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.