2025-12-04 7:35 PM - last edited on 2025-12-05 5:05 AM by mƎALLEm
New question split from this thread.
Hello,
Thank you for your response. I have double-checked and found that the 6.10 version also cannot be configured in this way. I will adopt the single-line mode on the next hardware version.
However, there is still a question regarding the configuration of can in version 6.16. Why must the sum of the two parameters in the following figure be 32? Otherwise, there will be a warning. In version 6.13, this issue does not exist.
The attachment contains the relevant IOC files.
2025-12-04 11:46 PM - edited 2025-12-05 12:44 AM
Hello @BJX
The CubeMX should allow (TX Buffers Nbr + TX FIFO Queue Elmts Nbr ≤ 32 ) instead of ((TX Buffer Nbr + TX Fifo Queue Elmts Nbr) == 32
A ticket (ID: 222211) has been escalated to the development team to address and correct this behavior.
Regarding this point :"Both TX and RX pins must be assigned simultaneously; otherwise, the UART peripheral cannot be enabled." : MX 6.10.0 and MX 6.16.0 are behaving the same way , in Asynchronous mode both pins are reserved.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.