2019-06-28 4:35 PM
I built a simple project using CubeMX(V5.2.1) for an STM32F103C8 (Blue Pill) , and compiled with Keil uVision5.
In CubeMX I enabled LSE and HSE, the SWD, and PA9 as a GPIO output. For everything else I used the CubeMX defaults.
I added the following code to main().
/* USER CODE BEGIN 2 */
volatile char ii=1;
while(1)
{
HAL_GPIO_WritePin (trigger_GPIO_Port, trigger_Pin, GPIO_PIN_SET);
HAL_Delay(ii);
HAL_GPIO_WritePin (trigger_GPIO_Port, trigger_Pin, GPIO_PIN_RESET);
HAL_Delay(100);
}
/* USER CODE END 2 */
In Operation, the output is set high, HAL_Delay(ii) is called, the output is set low and there is a delay of 100 milliseconds. Looking with a scope I always see an output pulse width of ii+1 milliseconds, for any ii. If I comment out the Hal_Delay(ii) line, the output pulse width drops to 2.5 usec, so its not the loop that's adding the extra millisecond.
So what am I missing here? The HAL manual is pretty clear about HAL_Delay(x) producing a delay of x ms.
Thanks for your help.
Dave
2019-06-28 4:58 PM
Well you can see the source.
Thing is, the method used the main loop in the delay routine can take approaching 0 ms if it enters just before the SysTick hits.
Realistically if want precision timing you're not using a tick of 1ms. Use something with finer granularity, or use a TIM to do the job at a HW level.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.