2020-09-13 9:56 AM
I'm creating a STM32Cube project, for the STM32H7B3I-DK. When selecting CMSIS Core and DSP in CubeMX, via Software Packs, then click ok, save, generate code, nothing happens. CMSIS or DSP lib aren't added. No module appears in the Software Package section of the .ioc editor.
If I close eclipse and open it again, the selected package sections are gone, not saved with the project.
STM32CubeIDE Version: 1.4.2
STM32CubeH7 Firmware Package V1.8.0 / 29-May-2020
CMSIS Release version : 5.7.0 Release date : 2020-04-09
2020-10-19 5:10 AM
Hello @Jan Cumps
I did the same scenario without getting issue. So, could you please share your project to check with.
Best regards,
Nesrine
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.