2023-08-21 4:02 PM - last edited on 2023-08-22 1:20 AM by KDJEM.1
Hi
The .mxproject is generated by STM32CubeMX in the code generation step. What is this file used for?
Thank you.
Pieter.
Solved! Go to Solution.
2023-08-22 2:14 AM
Hello @peks
First let me thank you for posting and welcome to ST Community.
The main purpose of the .mxproject file is to save parameters, configurations and pin mappings. This file is considered as the heart of the STM32 project. It contains information about the microcontroller selected like peripherals settings and middleware parameters.
Thx.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-22 2:14 AM
Hello @peks
First let me thank you for posting and welcome to ST Community.
The main purpose of the .mxproject file is to save parameters, configurations and pin mappings. This file is considered as the heart of the STM32 project. It contains information about the microcontroller selected like peripherals settings and middleware parameters.
Thx.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-22 5:08 AM - edited 2023-08-24 12:45 AM
@Mahmoud Ben Romdhane is there a more detailed or recent explanation on this file?
I use CubeMX for few years already, and .mxproject once was known to make trouble when re-generating projects, especially after move to a different path or rename. So I've learned to consider it harmful, delete it ASAP, and have never seen anything negative. Of course, not checking it into version control.
2023-08-23 7:58 PM
Thanks guys.
2024-02-23 7:30 AM
It is really a headache. When checkout to another git branch, file .mxproject frequently leads to compile failure.
2024-08-11 5:03 PM
Should .mxproject file be checked into source control? Or is it generated from .ioc file?
2024-08-12 2:57 AM
Cube creates this file when it edits or upgrades .ioc.
Don't check it in. I never check it, never seen any problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.