2019-02-12 2:32 AM
Hi am new to STM32,
I had generated USB device CDC example using STM32CubeMX 5.0.0 for STM32F427II and once i connect my DUT it show enumeration warning with following error, kindly see what i am doing wrong or can someone please share me just USB CDC device bare metal example code
Port1] : USB Serial Device
Is Port User Connectable: no
Is Port Debug Capable: no
Companion Port Number: 0
Companion Hub Symbolic Link Name:
Protocols Supported:
USB 1.1: yes
USB 2.0: yes
USB 3.0: no
---===>Device Information<===---
String Descriptor for index 2 not available while device is in low power state.
ConnectionStatus:
Current Config Value: 0x00 -> Device Bus Speed: Full (is not SuperSpeed or higher capable)
Device Address: 0x16
Open Pipes: 0
*!*ERROR: No open pipes!
===>Device Descriptor<===
bLength: 0x12
bDescriptorType: 0x01
bcdUSB: 0x0200
bDeviceClass: 0x02 -> This is a Communication Device
bDeviceSubClass: 0x02
*!*ERROR: bDeviceSubClass of 2 is invalid
bDeviceProtocol: 0x00
bMaxPacketSize0: 0x40 = (64) Bytes
idVendor: 0x0A12 = Cambridge Silicon Radio Ltd.
idProduct: 0x3039
bcdDevice: 0x0200
iManufacturer: 0x01
String Descriptor for index 1 not available while device is in low power state.
iProduct: 0x02
String Descriptor for index 2 not available while device is in low power state.
iSerialNumber: 0x03
String Descriptor for index 3 not available while device is in low power state.
bNumConfigurations: 0x01
---===>Full Configuration Descriptor<===---
===>Configuration Descriptor<===
bLength: 0x09
bDescriptorType: 0x02
wTotalLength: 0x0043 -> Validated
bNumInterfaces: 0x02
bConfigurationValue: 0x01
iConfiguration: 0x00
bmAttributes: 0xC0 -> Self Powered
MaxPower: 0x32 = 100 mA
===>Interface Descriptor<===
bLength: 0x09
bDescriptorType: 0x04
bInterfaceNumber: 0x00
bAlternateSetting: 0x00
bNumEndpoints: 0x01
bInterfaceClass: 0x02 -> This is Communications (CDC Control) USB Device Interface Class
bInterfaceSubClass: 0x02
bInterfaceProtocol: 0x01
iInterface: 0x00
-> This is a Communications (CDC Control) USB Device Interface Class
===>Descriptor Hex Dump<===
bLength: 0x05
bDescriptorType: 0x24
05 24 00 10 01
-> This is a Communications (CDC Control) USB Device Interface Class
===>Descriptor Hex Dump<===
bLength: 0x05
bDescriptorType: 0x24
05 24 01 00 01
-> This is a Communications (CDC Control) USB Device Interface Class
===>Descriptor Hex Dump<===
bLength: 0x04
bDescriptorType: 0x24
04 24 02 02
-> This is a Communications (CDC Control) USB Device Interface Class
===>Descriptor Hex Dump<===
bLength: 0x05
bDescriptorType: 0x24
05 24 06 00 01
===>Endpoint Descriptor<===
bLength: 0x07
bDescriptorType: 0x05
bEndpointAddress: 0x82 -> Direction: IN - EndpointID: 2
bmAttributes: 0x03 -> Interrupt Transfer Type
wMaxPacketSize: 0x0008 = 0x08 bytes
bInterval: 0x10
===>Interface Descriptor<===
bLength: 0x09
bDescriptorType: 0x04
bInterfaceNumber: 0x01
bAlternateSetting: 0x00
bNumEndpoints: 0x02
bInterfaceClass: 0x0A -> This is a CDC Data USB Device Interface Class
bInterfaceSubClass: 0x00
bInterfaceProtocol: 0x00
iInterface: 0x00
===>Endpoint Descriptor<===
bLength: 0x07
bDescriptorType: 0x05
bEndpointAddress: 0x01 -> Direction: OUT - EndpointID: 1
bmAttributes: 0x02 -> Bulk Transfer Type
wMaxPacketSize: 0x0040 = 0x40 bytes
bInterval: 0x00
===>Endpoint Descriptor<===
bLength: 0x07
bDescriptorType: 0x05
bEndpointAddress: 0x81 -> Direction: IN - EndpointID: 1
bmAttributes: 0x02 -> Bulk Transfer Type
wMaxPacketSize: 0x0040 = 0x40 bytes
bInterval: 0x00
2019-02-13 3:25 AM
Hi have generated code for CDC class virtual com, how does HID wil come in to picture (sorry my understating is wrong ) Could you please generate bare metal code for CDC class and send me if you wroking one or if you can generate for stm32f427II is my part number.
2019-02-13 7:13 AM
Hello @rangaec01 ,
Sorry, I comment on your discussion by miskake. I delete my answer as it is not apprpriate for your discussion.
For your case, I recommend you to take as reference the CDC example within STM32CubeF4 firmware package: STM32Cube_FW_F4_V1.23.0\Projects\STM324x9I_EVAL\Applications\USB_Device\CDC_Standalone
You can get inspired from this working CDC Standalone application and modify it depending on your needs.
Kind Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.