2020-01-10 1:23 AM
Hello,
in the last days I worked a lot with STM32CubeMX without any problems (STM32L432KC). I2C, SPI, UART and CAN work pretty well.
Now, I try to configure a simple PWM timer. When I only activate a timer (lets say TIM15 / The behaviour is the same for other timers) and I just generate code the following line will be created in main.c.
MX_TIM15_Init();This seems to be exactely the same like for all other peripherals... But when I compile the project, it says, that MX_TIM15_Init(); is not defined. An overall search confirms, that there is just a declaration in tim.h but no implementation.
Can anyone reproduce this issue?
Best regards!
Solved! Go to Solution.
2020-01-10 1:27 AM
2020-01-10 1:27 AM
It seems to be based on my IDE settings...
Problem can be closed.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.