2021-01-09 7:28 AM
At the end of the code generation process a message is produced that includes the text '..but MDK-ARM V5.27 project generation have a problem' (note: does this for all versions of the Keil IDE). It generates one file only; totally wrong. This behaviour occurs on: 1. Macbook Air, running High Sierra. 2. iMac running El Capitan. 3.iMac running Mojave. 4. Windows 10 running in Parallels on the Mijave iMac. However I have no problems with CubeMx v6.1.1 running on Windows 10 on a PC.
The issue appears to be related ONLY to the MDK-ARM IDE.
2021-01-21 2:05 AM
Hello @JCool.1
Can you please provide me more details about the issue (ioc, screenshot, log file..) ?
Thanks, Khouloud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.