2020-11-18 11:14 PM
Hi
I am facing issue with the "generate code" to generate the boiler plate code for the nucleo-f44re
here is the software that I am running with :
STMCubeMX_v6-0-1
Keil ARM-MDK 5.32
java version "1.8.0_271" (Java 8 I believe) , which is the recommended version of Java to run the CubeMX
*I even install the STM32CubeMX in the most shallow C directory "C:\<here>", so that I would not encounter any issues with too long path names*
This "generate code" issue comes right after I resolved another Issue with "installing stm32cube_fw_f4_v1252 libraries"
I managed to resolved this "stm32cube_fw_f4_v1252" library installing issue by manually going to the C:\\<User>\STM32Cube\Repository and manually unzipping the files .
could the problem of "generating the code", stem from this method of resolving "the stm32cube_fw_f4_v1252 library installing issue"?
are there anyone familiar with this issue of "project generation" or this software able to provide some assistance in resolving this issue ?
A swift reply and solution would be much appreciated :grinning_face:
Thanks
Solved! Go to Solution.
2020-11-19 5:10 AM
just a quick guide for any one visiting this thread:
go to control panel-> uninstall a program -> "search for the java version that is not supported, i.e. java 13" -> click uninstall
and also make sure to download the java 8 by "googling java 8"
It seems like it is possible to have multiple versions of java installed, like i had java 8 and java 13 installed. Therefore all i had to do is unistall java 13 and reboot my machine. and poof ! it works
thank you so much Nesrine.J for the quick and very accurate prescriptions !
2020-11-19 5:15 AM
Good News !
Best regards,
Nesrine
2020-11-19 5:16 AM
Good News !
Best regards,
Nesrine
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.