2021-05-18 6:09 AM
Hi,
With CubeMX I can adjust where the repositories are saved. This function is missing in CubeIDE and its also not using the same from CubeMX.
Because the saved files are huge, then I get problem when I login/logout in the company. Because the files are saved in the user directory, the first login/logout needed more than 1 hour because windows want to synchronise with the servers profile and the CubeIDE files are in the profile. The same happens again when i update the device database. This need a change or is there any way to change it?
At the other side, its without any reason to have the same files twice in the system!!?? Why both programms dont use the same data?
Osto
Solved! Go to Solution.
2021-05-18 6:20 AM
Of course you can use the same repository for CubeMX as for CubeIDE. But CubeIDE is based on Eclipse and therefore looks a bit different than CubeMX.
Just:
That easy...
Good luck!
/Peter
2021-05-18 6:20 AM
Of course you can use the same repository for CubeMX as for CubeIDE. But CubeIDE is based on Eclipse and therefore looks a bit different than CubeMX.
Just:
That easy...
Good luck!
/Peter
2021-05-18 7:18 AM
Thanks a lot. Its working.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.