2018-03-31 3:54 PM
Hello,
I just faced a problem in STMCube MX for STM32L053R8T6, there is no option to select alternative function OPEN DRAIN output for LPUART1.
I see the option for USART1 or USART2 GPIO settings but not for LPUART1.
I First thought that option is not available for LPUART peripheral, so checked all datasheet's related pages ... but didn't find any note about it.
Finally i changed the generated code (LPUART1 MspInit part) manually and set the TX pin of LPUART1 output mode to GPIO_MODE_AF_OD, then it worked.
I just wanted to inform you to correct this bug in the software for future.
The Installed package for L0 series in STMCube is V1.10.0 (The last update).
Thanks & Regards.
#push-pull-output-or-open-drain-output #lpuart #stmcube-mx #stm32l0-lpuart-output-mode2018-04-02 8:09 AM
Hello
fallah.omid
Thank you for your reported issue.This is highlighted internally to CubeMx team.
Best Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.