2023-01-06 12:44 AM
Hi everyone,
I'm working on a project with an STM32L072C6T6.
I'm using LPUART1 DMA to get data from my LPUART with interrupt when the bus go idle.
My soft working when, after power on the device, i push the reset button of the MCU. All start correctly.
But when I try turn on my device with only power ON, no interrupt from LPUART occur.
Do you have advice that can put me on a way of a solution ?
I attached CubeMX configuration screen and function that i use to use the LPUART DMA.
Best regards,
Lam
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
{
if (huart->Instance == LPUART1)
{
//do something
printf("LPUART1\r\n");
/* start the DMA again */
memset(lpuart1_Rx_data, 0, sizeof(lpuart1_Rx_data));
HAL_UARTEx_ReceiveToIdle_DMA(&hlpuart1, lpuart1_Rx_data, sizeof(lpuart1_Rx_data));
__HAL_DMA_DISABLE_IT(&hdma_lpuart1_rx, DMA_IT_HT);
}
if (huart->Instance == USART1)
{
//printf("INT USART1\r\n");
/* start the DMA again */
memset(usart1_Rx_data, 0, sizeof(usart1_Rx_data));
HAL_UARTEx_ReceiveToIdle_DMA(&huart1, usart1_Rx_data, sizeof(usart1_Rx_data));
__HAL_DMA_DISABLE_IT(&hdma_usart1_rx, DMA_IT_HT);
}
}
//-------------------------------
int main(void)
{
/* USER CODE BEGIN 1 */
clear_led();
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_I2C1_Init();
MX_LPUART1_UART_Init();
MX_USART1_UART_Init();
MX_ADC_Init();
MX_USB_DEVICE_Init();
MX_LPTIM1_Init();
MX_RTC_Init();
/* USER CODE BEGIN 2 */
Init_Context();
//Enable LPUART for RF interrupt
HAL_UARTEx_ReceiveToIdle_DMA(&hlpuart1, lpuart1_Rx_data, sizeof(lpuart1_Rx_data));
__HAL_DMA_DISABLE_IT(&hdma_lpuart1_rx, DMA_IT_HT);
//Enable USART1 for Keyboard RFID
HAL_UARTEx_ReceiveToIdle_DMA(&huart1, usart1_Rx_data, sizeof(usart1_Rx_data));
__HAL_DMA_DISABLE_IT(&hdma_usart1_rx, DMA_IT_HT);
//verify if DMA is correctly init
getDMA_init();
//test_main();
#ifdef DEBUG_PRINT
printf("*** DEBUG FIRMWARE ***\r\n");
#endif
while(1)
{
}
}
//------------------------------------
static void MX_LPUART1_UART_Init(void)
{
/* USER CODE BEGIN LPUART1_Init 0 */
/* USER CODE END LPUART1_Init 0 */
/* USER CODE BEGIN LPUART1_Init 1 */
/* USER CODE END LPUART1_Init 1 */
hlpuart1.Instance = LPUART1;
hlpuart1.Init.BaudRate = 9600;
hlpuart1.Init.WordLength = UART_WORDLENGTH_8B;
hlpuart1.Init.StopBits = UART_STOPBITS_1;
hlpuart1.Init.Parity = UART_PARITY_NONE;
hlpuart1.Init.Mode = UART_MODE_TX_RX;
hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&hlpuart1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN LPUART1_Init 2 */
/* USER CODE END LPUART1_Init 2 */
}
//---------------------------------
static void MX_DMA_Init(void)
{
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
/* DMA interrupt init */
/* DMA1_Channel2_3_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Channel2_3_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel2_3_IRQn);
/* DMA1_Channel4_5_6_7_IRQn interrupt configuration */
HAL_NVIC_SetPriority(DMA1_Channel4_5_6_7_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Channel4_5_6_7_IRQn);
}
//----------------------------
void getDMA_init(void)
{
//Waiting DMA hardware initialization
uint8_t draw_wait_state = 0;
uint32_t counter;
HAL_DMA_StateTypeDef test;
uint32_t test2;
test = HAL_DMA_GetState(&hdma_lpuart1_rx);
printf("dma lpuart1 : %x", test);
test = HAL_DMA_GetState(&hdma_usart1_rx);
printf("dma usart1 : %x", test);
test2 = HAL_DMA_GetError(&hdma_lpuart1_rx);
printf("dma lpuart1 error : %lu", test2);
test2 = HAL_DMA_GetError(&hdma_usart1_rx);
printf("dma usart1 error: %lu", test2);
}
2023-01-11 6:17 AM
News about my problem,
I have try to get information about my LPUART state. So i use this functions to get informations : HAL_UART_GetState(&hlpuart1) and HAL_UART_GetError(&hlpuart1).
I use this functions after uart init and i ahve this results : lpuart 1 state : 34 lpuart 1 error : 0
I use this just before my function that want to receive and send data throught LPUART1 and i obtain this results : lpuart 1 state : 32 lpuart 1 error : 0
I understand that i have an error on my LPUART1 apparently. But i don't understand the cause and why this occur only sometimes.
I joined below my code to check error.
Do you have advice about this error ?
void getDMA_init(void)
{
//Waiting DMA hardware initialization
uint8_t draw_wait_state = 0;
uint32_t counter;
HAL_DMA_StateTypeDef test;
uint32_t test2;
HAL_UART_StateTypeDef test3;
test = HAL_DMA_GetState(&hdma_lpuart1_rx);
printf("dma lpuart1 : %x ", test);
test = HAL_DMA_GetState(&hdma_usart1_rx);
printf("dma usart1 : %x ", test);
test2 = HAL_DMA_GetError(&hdma_lpuart1_rx);
printf("dma lpuart1 error : %lu ", test2);
test2 = HAL_DMA_GetError(&hdma_usart1_rx);
printf("dma usart1 error: %lu \r\n", test2);
test3 = HAL_UART_GetState(&hlpuart1);
printf("lpuart 1 state : %lu ",(uint32_t)test3 );
printf(" lpuart 1 error : %lu \r\n", HAL_UART_GetError(&hlpuart1));
}
2023-02-21 1:51 AM
Dear @MLam
Regarding UART state values you mentioned, i don't think this indicates an error.
32 => 0x20 indicates Initialisation has been done an no TX or RX activity is ongoing. No error reported.
34 => 0x22 indicates Initialization is done, and a RX process is ongoing.
Regarding your problem, when nothing seems to appear on reception side, could you check the LPUART ISR register content when this occurs ? One hypothesis could be that Overrun flag is set, preventing any further reception until it is cleared.
Just an idea ...
Hope this helps
2023-02-21 2:02 AM
Hello,
Thanks for you return,
I found a solution to solve my problem when my device boot,
if (HAL_UART_GetState(&hlpuart1) == 32) // on power-on LPUART/DMA meet problem to start interrupt maybe due of power-on of the module connected so we need to reinitialize LPUART and DMA
{
HAL_UART_Abort_IT(&hlpuart1);
HAL_UART_DMAStop(&hlpuart1);
MX_LPUART1_UART_Init();
//Enable LPUART for RF interrupt
HAL_UARTEx_ReceiveToIdle_DMA(&hlpuart1, lpuart1_Rx_data, sizeof(lpuart1_Rx_data));
__HAL_DMA_DISABLE_IT(&hdma_lpuart1_rx, DMA_IT_HT);
}I'm agree that not the better solution but that allow my program to receive the frames with interrupt.
Since this time my program has evolve and i start with USART and after LPUART, i don't need to use this code and i don't meet this error.
Best regards,
MLam
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.