2019-04-11 8:17 AM
Hey everybody.
i have the following problem, after updating my System Workbench for STM32 and my STM32CubeMX I got the same error every time (see below). When I create a project with Cube, the first time works well. But if I want to add some options like SPI and generate a second time, CubeMx deletes all the code in STM32H743ZITx_FLASH.ld. Which leads to an error after build and run like this:
** Programming Finished **
** Verify Started **
Error: checksum mismatch - attempting binary compare
diff 0 address 0x00000000. Was 0x2d instead of 0xf8
diff 1 address 0x00000001. Was 0xa8 instead of 0xb5
diff 2 address 0x00000002. Was 0x03 instead of 0x00
diff 3 address 0x00000003. Was 0x67 instead of 0xbf
diff 4 address 0x00000004. Was 0xc9 instead of 0xf8
diff 5 address 0x00000005. Was 0xb8 instead of 0xb5
diff 6 address 0x00000006. Was 0x64 instead of 0x00
diff 7 address 0x00000007. Was 0x19 instead of 0xbf
No more differences found.
** Verify Failed **
shutdown command invoked
It is of course possible for me to avoid this error by manually adding the code again, but this can't be intentional ?!
Is this a bug from the update ?
My program versions are:
SW4STM32: Neon.3 Release (4.6.3)
STM32CubeMX: 5.1.0 and firmware: 1.3.2
Hardware: NUCLEO-H743ZI Board
Thanks for help
regards
Rene
2019-04-21 10:56 AM
I hope this one gets answered, I suffer from the very same problem on NUCLEO-F746ZG and DISCO-F746G. The interesting thing that after build I can see the following output in system workbench:
Finished building target: test.elf
make --no-print-directory post-build
Generating hex and Printing size information:
arm-none-eabi-objcopy -O ihex "test.elf" "test.hex"
arm-none-eabi-size "test.elf"
text data bss dec hex filename
8 0 0 8 8 test.elf
As I see the entire size of the elf is 8 bytes. And this always occures after i modify something in cubeMX. Even if I change it back it can't be fixed.
CubeMX: 5.1.0
2019-05-26 8:11 AM
I get the same problem. Hope somebody could help. My temporary solution: delete STM32F091RCTx_FLASH.ld before regenerate the source from cubemx.
2019-09-16 10:23 AM
Had the same problem, temporary solution of @Jean-Sébastien Castonguay works fine...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.