2020-08-25 7:22 AM
Getting started with STM32H7, faced a problem.
Ive worked for a long time with STM32F4 in Keil uVision (version 5.24.2.0), used a "classic" option, configuration via RTE_Device.h. Worked perfect.
Now I dont have such option with STM32H7, only CubeMX, and adventures began.
Created project with CubeMX, project building successfully. But when Im trying to add something i.e. filesystem, rtos, etc, it says that it is necessary to start CubeMX (again), and it starts complete different CubeMX project, a new one. Ok, fine, It adds a new main.c, stm32h7xx_it.c, etc. Obviously fails to build.
Creating project with Keil looks makes a bit more sense, but still unable to build up a complete application, got the same issue as
https://community.st.com/s/question/0D50X00009kHvWr/keil-mdk-and-st32cubemx-not-interacting
Is there a way to not use CubeMX in any way?
Solved! Go to Solution.
2020-08-26 2:07 AM
Updating Keil uVision to V5.31.0.0 worked
2020-08-25 8:21 AM
Can use the H7 HAL directly, should be MDK projects and templates in the example trees.
2020-08-26 2:07 AM
Updating Keil uVision to V5.31.0.0 worked
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.