2019-07-10 2:45 AM
Hi,
Can I somewhere find an example for STM32F4 + SDIOCard(Bluetooth/Wifi) ??? (It's not a SD-Card and not a MM-Card)
It seems, CubeMX can only generate HAL for SDC and MMC based on Hardware Module SDIO.
SDIO-Card needs different initiallization and data Exchange CMD's … e.g. starting initialization with CMD5 ...
Very Best Thanks for any Help!
2019-07-10 8:10 AM
CubeMX isn't going to provide a workable example.
You're going to need ro read the protocol manual for your device(s), and perhaps Linux drivers your can examine/port.
You'll then need to understand the HAL peripheral level SDIO functions as the higher level SD/MMC support routines likely aren't directly suitable. They will provide some understanding of commands/protocols, and peripheral expectations.
Perhaps you can find a third-party library you can license, or contractors with specific experience.
Expect to have to do some work.
2021-10-29 5:12 AM
Hi, now end of 2021 and I can't find any example of WLAN by SDIO. Do you have any updates?
2021-10-29 7:04 AM
Yeah, clearly a pretty niche use case, or one where companies have developed closed solutions on their own dime, The size of Windows or Linux drivers for the card should be indicative of the complexity and host side foot-print.
Have the embedded sw engineers on the project work the documentation for the WLAN card(s) and peripheral level examples on the SDIO/SDMMC side
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.