2021-08-13 7:59 AM
I have this odd behaviour, where the ADC1 works with a fresh .ioc configuraion but does not when I configure additional peripherals.
The working case: (see attached f373rb_playground.ioc)
Where I configure 4 channels of the ADC1 to work in scan mode together with the DMA in circular mode.
/* USER CODE BEGIN PV */
volatile uint16_t ADC_Buf[4 * 16];
/* USER CODE END PV */
/* USER CODE BEGIN 2 */
HAL_ADC_Start_DMA(&hadc1, ADC_Buf, 4*16);
HAL_ADC_Start_IT(&hadc1);
/* USER CODE END 2 */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
printf("%d\t%d\t%d\t%d\n", ADC_Buf[0], ADC_Buf[1], ADC_Buf[2], ADC_Buf[3]);
HAL_Delay(100);
}This is working and I get a continuous stream of ADC values like:
1615 313 0 2370
1615 314 0 2369
1615 313 0 2368
1612 313 0 2367
However, when I configure more peripherals (see attached f373rbt_SGmini_MK2.ioc) the same code above does not work and just produces empty values like so:
72 0 0 0
72 0 0 0
72 0 0 0
72 0 0 0
72 0 0 0
I see two possibilities:
If it is the latter, what could interfere with it?
All I do is configure the peripherals (and initialize them in the code) but I do not start anything yet. I am not aware of any TIMer being used by the ADC as I have none configured in the first example. I also don't use any other DMA channels.
Version: 1.7.0
Build: 10852_20210715_0634 (UTC)
STM32Cube FW_F3 V1.11.3
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.