2017-09-07 4:48 AM
Hello,
I'm using STM32F103RBT6 for my project, I've designed a custom board.
I'm using cubemx to generate the basic code and Atollic for debugging.
I'm reading the switches using external interrupt. In the external interrupt call back, I'm starting a timer.
In the timer interrupt handler, I'm doing some work.
I've kept the timer timeout period to 2 seconds.
My problem is whenever the code is started to run for the first time and when I press the switch, the code immediately goes to the timer interrupt handler. This happens only once for the first time. After this, whenever I press the switch, code goes to the timer interrupt in 2 seconds which is correct.
Why does it go immediately goes to the interrupt handler for the first time and then works fine thereafter??
I've attached the c file for reference.
Is there any changes to be made??
Please suggest.
Regards
Praveen
#cubemx-project #mcu #stm #stm32f1032018-04-30 10:15 AM
I exactly have the same issue .. When I set the TIM_CEN bit , MCU immediately goes to the interrupt routine ,even though the overflow hasn't occured yet ..But for the next timer stopping and startings , it doesn't give me a problem .. An answer would be appreciated so much ..
2018-04-30 10:44 AM
Check TIM_SR after setting the timer up. It's probably nonzero; if so, clear it.
JW
2018-04-30 12:47 PM
I did ... But still no luck ..
2018-05-01 3:51 AM
Well , I gave it a try by forcing the software in a different way ..Here is the Timer_Config function I use to configure the timer ..And now it works as I expect ...
/*¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨*/
void Tim1_Config(void)
{TIM1->ARR=7199; //FreqTIM1->PSC=499; //50 mSec Interrupt Period
TIM1->CR1=(uint16_t)0x0000;
TIM1_UIE=1; NVIC_SetPriority(TIM1_UP_IRQn,1); while(TIM1_UIF) TIM1_UIF=0; //Clear TIM1_UIF TIM1_CEN=1; //Start TIM1 while(!TIM1_UIF) __NOP(); //Wait till TIM3_UIF goes high while(TIM1_CEN) TIM1_CEN=0; //Stop the TIM3 while(TIM1_UIF) TIM1_UIF=0; //ClearArray TIM3_UIF while(NVIC_GetPendingIRQ(TIM1_UP_IRQn)) //Clear pending interrupt flag NVIC_ClearPendingIRQ(TIM1_UP_IRQn); NVIC_EnableIRQ(TIM1_UP_IRQn); //Now it is safe to enable the timer;}/*¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨¨*/2018-05-01 2:22 PM
Nice, but a bit more complicated than needed:
- you don't need to run the timer until update (in order to 'activate' the prescaler); you can force update by setting TIMx_EGR.UG
- if you don't enable the update interrupt in DIER (that's presumably what you do by TIM1_UIE=1;) before the forced update, but only after the update and after the SR has been cleared (TIM1_UIF=0;), you don't need to clear the pending interrupt flag by NVIC_ClearPendingIRQ().
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.