2018-04-11 2:48 AM
Hi guys.
I'm working in a STM32L433RCTP based project.
The code generated by the Stm32CubeMX for clock configuration has no value set for the PLL-M prescaler in the PLL struct, see original code:
----------------------------------
/**Initializes the CPU, AHB and APB busses clocks
*/ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSE; RCC_OscInitStruct.HSEState = RCC_HSE_ON; RCC_OscInitStruct.HSI48State = RCC_HSI48_ON; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; RCC_OscInitStruct.PLL.PLLN = 10; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7; RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }----------------------------------
I fixed it, by adding the folowing line:RCC_OscInitStruct.PLL.PLLM = 1;Even with PLLM prescalers set with different values than 1, CubeMX will forget to add the line.If I don't add the line, the program freezes at the function call of HAL_RCC_OscConfig(..).The bug seems to be occured in a different configuration in the past, too, see:
#system_clock #cubemx-v4.25.0 #systemclock_config #stm32l433rctx2018-04-12 12:31 AM
We have the same issue with the same workaround here in our project for an STM32L0...
Please fix that!
2018-04-12 12:44 AM
Same problem with the STM32L452
2018-04-12 12:55 AM
Hello,
We
confirm that PLLM parameter
is no more generate for STM32L4 in the CubeMX
version 4.25
.T
his bug passed internally to CubeMx team for fix in coming release.Sorry for such inconvenience.
Best Regards,
Imen
2018-04-12 1:50 AM
Hello H.K,
Thanks for your feedback.
The issue will be fixed next CubeMX release.
Please feel free to contact me for further details.
Best regards,
Houda
2018-04-12 2:57 AM
Hello
Schwarzl.Markus
,Could you please confirm that you reproduced this issue with STM32L0 using the last CubeMx version 4.
Otherwise, please share your ioc for more check from our CubeMX team.
Best Regards,
Imen
2018-04-12 3:00 AM
Hi Imen,
sorry, this was a typo on my side! It is an STM32L476G!
Thanks,
Markus
2018-05-03 7:52 AM
4.25.1 fixing this issue will be available by the end of this week
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.