2019-02-26 11:50 AM
I opened an older project which was created with 5.0.1, and the newest CubeMX shows an error for this option in ADC. But this option is correct. I tried to create a new project, and I wasn't able to enable this option here.
Solved! Go to Solution.
2019-04-24 1:11 AM
So it means, this issue is fixed too? It's mainly related to low layer driver, with HAL it worked before.
2019-04-24 4:14 PM
2019-04-25 12:08 AM
@Jeff Gros
You're Right, this issue is already reported and it wil be fixed in the next release. Sorry for any inconvenience this may have brought.
Best Regards
khouloud.
2019-04-26 12:09 AM
Yes, this is fixed. I can confirm it too!
But you can't measure temp sensor with vref with LL, because freshly generated code will only enable measuring vrefint. Tested with 5.2.0.
2019-08-06 6:42 AM
Hello I was working in Mxcube 5.01 and I updated to 5.3.0 and I can not set the parameter DMA continues Request to ENABLE only Disable shows up.
I was using and project that I am working, but I created a new one from the scratch and I can no set this option. I ma using STM32F446ZEJx.
Is this bug not fixed for this MCU ?
Thank you
2019-08-06 6:52 AM
When I open my old Project I clicked in migrate project, I got my old Ioc file and I did not click Migrate I just clicked in Download package and this allow me to change this DAM setting, but if i do i new project I can not change it using STM32F446ZEJx
Thank you
2019-08-06 7:25 AM
hello @mospi , I will check it, please share your ioc file.
Best Regards,
Khouloud.
2019-08-07 9:44 AM
2019-09-03 5:23 AM
I have the same problem with SMT32F446RE.
2019-09-03 6:30 AM
Hello the Ioc was shared like month ago.
can you tell us if this bug is fixed or how can we go around this.
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.