2018-02-07 8:11 AM
Hi,
I have a problem with STMCubeMx v4.24.0.
My problem is : I cannot open a new project created with STM32CubeMx v4.24.0. This project was created from scratched. After I finish editing the file, I save it and close the software. When I re-open the project file, nothing happens. My mouse cursor is transformed into a blue circle (busy). It's impossible to close the tool without forcing (ctrl-alt-supr or task manager).
In STM32CubeMX.log I have these errors :
2018-02-07 16:57:00,996 [INFO] ImportTextPane:155 - (OptionalMessage_ERROR) IP (RCC) : Parameter (ADCFreq_Value) has invalid value (96000000)
2018-02-07 16:57:00,997 [INFO] ImportTextPane:155 - (OptionalMessage_ERROR) IP (RCC) : Invalid parameter (FamilyName)When I open the .ioc file, I have these value for these attributes :
RCC.ADCFreq_Value=96000000
...
RCC.FamilyName=M
I am sure to configure correctly my clocks before I close the file. My ADC clock is 80MHz and not 96MHz. If I change 96000000 by 80000000 the first error (
(OptionalMessage_ERROR) IP (RCC) : Parameter (ADCFreq_Value)....
) disappears.For the second error (FamilyName), I don't know the expected value I have to put there.
I don't know why these values changed.
Did anyone ever have this problem or can help me to understand this case?
Thanks a lot.
Regards
What I already did :
Context :
The .ioc file is in attached file.
#program-stuck #cubemx-4.24 #stm32cubemxSolved! Go to Solution.
2018-03-20 9:41 AM
Hello
andrianina.andriaman
,Dr_b.Dominik
andErol.Mehmet_Akif
,This issue is now fixed in the current CubeMX release.
Please, upgrade with CubeMX4.25 if not already done.
BR. Jeanne
2018-02-07 9:23 AM
Hello
andrianina.andriaman
,This issue is already raised internally to CubeMx team for fix.
Best Regards
Imen
2018-02-07 10:51 AM
Hi Imen,
Thanks for your answer! In the meantime, how can I go forward.
Is it possible to downgrade the software for having a previous stable version.
Kind regards
2018-02-08 2:01 AM
For those who are interested, alder version of STM32CubeMx is avalaible here :
2018-02-17 11:39 AM
I've got same issue with re-opening project. After downgrading to 4.23.0 I still can't open the project, because it was created in newer version. It is possible to import the project, but there are various errors and also this version of CubeMX uses older firmware package.
I hope this issue will be fixed soon, as I am stuck right now.
2018-02-22 7:37 AM
Hello
Dr_b.Dominik
andAndrian Andria,
This issue is well known by our development team, sorry for any inconvenience it may cause.
I confirm that the correction will be available in the next CubeMX release.
BR. Jeanne
2018-02-23 1:36 AM
STM32CubeMX, being an impressive and very useful peace of software, continues to constantly deliver new severe bugs with each version, as if a permanent beta-version quality product.
I understand that where there is any kind of new complicated code there are going to be bugs. Why don't you use the standard practice of releasing beta or release candidate versions before a real release? The brave and those hungry for new features could hunt for and report the bugs (and we need a dedicated bug-reporting platform) in the beta version. Then you would fix those bugs without adding any new features and make a release (while adding new features to the next beta version).
2018-03-08 10:50 PM
I have the exact same problem with the addition that i cannot open projects created with 4.23.0 as well.
Please issue a quick fix for this. I am trying to find 4.23.0 for now. I hope that will open the projects.
2018-03-20 9:41 AM
Hello
andrianina.andriaman
,Dr_b.Dominik
andErol.Mehmet_Akif
,This issue is now fixed in the current CubeMX release.
Please, upgrade with CubeMX4.25 if not already done.
BR. Jeanne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.