2018-01-30 7:59 AM
Hi,
when I generate a example for the nucleo32 L432kc everything is fine, until I check the option freeRTOS
After this the includes are not correct anymore:
>>>>>
Src\freertos.o: In function `StartDefaultTask':
E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/freertos.c:118: undefined reference to `HAL_GPIO_TogglePin'E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/freertos.c:119: undefined reference to `osDelay'Src\freertos.o: In function `MX_FREERTOS_Init':E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/freertos.c:99: undefined reference to `osThreadCreate'Src\gpio.o: In function `MX_GPIO_Init':E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/gpio.c:80: undefined reference to `HAL_GPIO_WritePin'E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/gpio.c:87: undefined reference to `HAL_GPIO_Init'Src\main.o: In function `SystemClock_Config':E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/main.c:156: undefined reference to `HAL_RCC_OscConfig'E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/main.c:170: undefined reference to `HAL_RCC_ClockConfig'E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/main.c:177: undefined reference to `HAL_PWREx_ControlVoltageScaling'E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/main.c:184: undefined reference to `HAL_RCC_GetHCLKFreq'E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/main.c:184: undefined reference to `HAL_SYSTICK_Config'E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/main.c:188: undefined reference to `HAL_SYSTICK_CLKSourceConfig'E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/main.c:191: undefined reference to `HAL_NVIC_SetPriority'Src\main.o: In function `main':E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/main.c:92: undefined reference to `HAL_Init'E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/main.c:115: undefined reference to `osKernelStart'Src\stm32l4xx_it.o: In function `SysTick_Handler':E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/stm32l4xx_it.c:157: undefined reference to `osSystickHandler'Src\stm32l4xx_it.o: In function `TIM7_IRQHandler':E:\Workspaces\Atollic9\432kcTest\Debug/..\Src/stm32l4xx_it.c:178: undefined reference to `HAL_TIM_IRQHandler'collect2.exe: error: ld returned 1 exit status<<<<<<<<<<
when I copy the same sourcecode into a emtpy project, insert the symbols and directories, setup the mcu -->
Generate build reports...
Print size information text data bss dec hex filename 52544 20 4044 56608 dd20 L432KC.elfPrint size information doneGenerate listing fileOutput sent to: L432KC.listGenerate listing file doneGenerate build reports doneI think the includes are not linked correct.
regards
Roger
#cubemx-4.24 #atollic #freertosSolved! Go to Solution.
2018-03-20 9:37 AM
Hello
Heil.R
,
massicotte.mathieu
andkelly.andrew
,This issue is now fixed in the current CubeMX release.
Please, upgrade with CubeMX4.25 if not already done.
BR. Jeanne
2018-01-30 7:23 PM
I'm experiencing what looks like the same after the 4.24.0 CubeMX update.
Create a new stm32f427ii project in CubeMX with the TrueStudio toolchain setting.
Generate code - open TrueSTudio and build the project .. everytyhing's fine.
Add FreeRTOS to the CubeMX project (use one of the MCU Timers for the SYS Timebase Source)
Generate code - open TrueStudio and build. This time it fails to build with a heap of FreeRTOS and HAL calls broken.
If I go to the project in TrueStudio, the Drivers and Middlewares folder contents are incomplete ...
right-click on the Drivers directory and Delete it
right-click on the Middlewares directory and Delete it
I might need to right-click on the project and select Refresh, but often TrueStudio does its own refresh before I need to
TrueStudio reacquires the Drivers and Middlewares directories and their contents.
Build now works correctly ......
and the built s/w appears to be running correctly (I haven't yet run a full regression test though).
2018-02-06 2:56 PM
Same thing here. Deleting the virtual folders seems to do the trick.
2018-02-07 1:51 AM
Hello,
We confirm this issue and
raise it internally to CubeMX team for fix.
Sorry for any inconvenience it may bring for you.
Best Regards,
Imen.
2018-03-20 9:37 AM
Hello
Heil.R
,
massicotte.mathieu
andkelly.andrew
,This issue is now fixed in the current CubeMX release.
Please, upgrade with CubeMX4.25 if not already done.
BR. Jeanne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.