2020-03-10 9:33 AM
I have a project, I'm in the Pinout & Configuration view, everything is serene and placid.
I click on a pin and CubeMX brings up a list of possible configurations for a pin.
Meanwhile, in the background, I hear my fans spin up. Click over to Activity Monitor and STM32CubeMX is taking 113% (1 full thread plus a bit) of CPU time.
Click away and everything is sunshine and unicorns again.
How did I notice this? Well I came in this morning to find my laptop with 7% left on the battery. My laptop will actually pull more current than the charger can provide, then it starts drawing down the battery. Eventually it will shut itself down. That's a lot of power being sucked to display a text picker. (no I don't need to bike shed or shave yaks about Apple's charging system)
Just thought you'd like to know.
Andrei from The Great White North
2020-03-10 10:29 AM
Java. It's about brewing coffee, right?
Get just the pins/functions table and do it in a spreadsheet processor.
Or print it out and do it with the old fashioned pencil. That is hard to beat when it comes to power consumption.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.