2019-02-22 8:22 AM
Hi all,
I'm trying to set-up a simple USB read/write on our STM32F746G-Disco board using the FullSpeed OTG... but so far it seems that the code generated by CubeMX does not really work...
If I'm not wrong, CubeMX in case of USB MSD enable the DMA template by default, but then it does not copy the usbh_diskio_dma.c and usbh_diskio_dma.h in the project folder.
After disabling the DMA, I can now detect when an USB key is attached and I can see that it is enumerated, but then It fails to open any file after the f_mount() with the error "FR_NOT_ENABLED".
It seems that I'm having the same issue described in: http://www.openstm32.org/forumthread3205
Below is a small log.
Best Regards,
Giampaolo
-----------
System initialized
StartDefaultTask
APPLICATION_START
FatFs initialized!
USB Device Attached
PID: 5571h
VID: 781h
Address (#1) assigned.
Manufacturer : SanDisk
Product : Cruzer Fit
Serial Number : 4C530001010701111474
Enumeration done.
This device has only 1 configuration.
Default configuration set.
Switching to Interface (#0)
Class : 8h
SubClass : 6h
Protocol : 50h
MSC class started.
APPLICATION_READY
opening file...
Cannot Open 'USBHost.txt' file: FR_NOT_INITIALIZED
2019-02-22 8:24 AM
...by the way... we are using STM32CubeMX + Atollic
2019-02-25 3:10 PM
Did you use delayed initialization with f_mount (at the top of your app, maybe where you reported FatFs initialized!), or forced mount after the USB device was enumerated?
2019-02-27 12:45 AM
Hello Dave,
I've done various test with both initialization modes (delayed and immediate) but with the same results... but...
yesterday finally I've found the problem and, hopefully, a solution:
In the file usbh_msc.c, the function USBH_MSC_ClassRequest() is calling USBH_MSC_BOT_REQ_GetMaxLUN()... which in my case it was stuck returning USBH_BUSY status.
By changing a single line as suggested here:
i.e. by changing this line as shown:
if((status == USBH_NOT_SUPPORTED) || (status == USBH_BUSY))
everything is now working as expected, both on a very old 512MB Apacher and on two new 16/32GB SanDisk USB mass storage pen-drive.
thanks for the help,
Giampaolo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.