2021-01-07 1:48 AM
I am very new to the STM32 development board and am using the STM32F407VG. I wish to connect a RFID Scanner to SPI2 and looking at the Pin Description Table (pages 21->23 in the STM32F4 users manual), I cannot see if there are specific pins to be selected for SPI2 Chip-Select-Pin setup (I think I can use PB9 but am not sure). I think I'm correct to use SPI2->PC2 = MISO, SPI2->PC3 = MOSI & SPI2-> PB10 = CLK. Has anyone dealt with this issue that can help me to know if I have to select specific pin please?
Solved! Go to Solution.
2021-01-07 2:18 AM
Hello BAher.1,
Welcome to our Community :)
You will find in the STM32F4 Data Sheet : Table 7. STM32F40xxx pin and ball definitions, specific pins for each peripheral.
Hope this answers your question.
If yes, please click on the Select as Best button on my reply . This will help other members of the community find this solution more quickly
Khouloud.
2021-01-07 2:18 AM
Hello BAher.1,
Welcome to our Community :)
You will find in the STM32F4 Data Sheet : Table 7. STM32F40xxx pin and ball definitions, specific pins for each peripheral.
Hope this answers your question.
If yes, please click on the Select as Best button on my reply . This will help other members of the community find this solution more quickly
Khouloud.
2021-01-07 3:29 AM
Thank you for the fast reply and all your help Khouloud =)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.