2018-09-27 8:58 AM
Reason for the question:
We want to generate two different hardware settings (CubeMX projects) into one software program running on a STM32 controller. Then at startup, the controller finds out, which HW configuration it has to use and uses just one of the two available ones to startup/init the system peripherals/hardware.
Thanks for any help.
2018-09-27 10:14 AM
Make two separate projects, burn them into separate flash areas + small bootloader which will probe hardware and select one variant ?
--pa
2018-09-27 10:24 AM
Sounds like a rats nest of a problem better solved by some careful merging.
I'd rather the engineers focus on generating solid test coded.
2018-09-29 11:21 PM
Hi Pawel
thanks for the idea. We will look into this in more detail.
We thought there might be a solution using the templates in STM32CubeMX, but it seems that there is no clean solution from the tool itself.
Thanks again.
2023-02-12 1:13 AM
It's surprising that this is not possible. I have a similar case...a library with a default CubeMX configuration built-in, with the desire to be able to override this by adding a CubeMX project in the application directory.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.