2020-08-25 3:17 AM
2020-09-02 3:27 AM
Hi @AXu.1 ,
STM32CubeMX is available as standalone software running on Windows®, Linux® and macOS® operating systems and 64-bit Java Runtime environment.
Here the installation steps as described in UM1718:
In case of error, try one of the following fixes:
- $sudo xattr -cr ~/SetupSTM32CubeMX-VERSION, or
- launch the .exe file with the following command: sudo java -jar SetupSTM32CubeMX-4.14.0.exe.
4. Upon successful installation of STM32CubeMX on Windows, STM32CubeMX icon is displayed on your desktop and STM32CubeMX application is available from the Program menu. STM32CubeMX .ioc files are displayed with a cube icon. Double-click them to open up them using STM32CubeMX.
5. Delete the content of the zip from your disk.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-09-02 5:15 PM
Hi! Amel,
Thanks for your support. I've installed STM32CubeMX in Windows 10 and learnt its functions. I'm waiting for another reply from STM concerning how to combine projects when there are more than one project. Whenever I get that reply I'll try to install STM32CubeMX again in Mac OS.
Regards,
Adam
2020-09-04 9:08 AM
Hi @AXu.1 ,
Are you speaking about this discussion? I agree with @TDK's answer there and I suggest you to submit your proposal in Idea Zone.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.