2025-11-18 2:17 AM - last edited on 2025-11-20 3:06 AM by mƎALLEm
Split from this thread.
Hi mƎALLEm, Thanks for this reply and confirming that the OSC_OUT can be used as GPIO when HSE in bypass mode. Can you please advise I do I set this as a GPIO? CubeMX does not allow me to configure this pin. Should this be hand coded to make this possible? Thanks. Regards Billy
2025-11-18 2:26 AM - edited 2025-12-01 12:28 AM
@BPart.1 wrote:
CubeMX does not allow me to configure this pin. Should this be hand coded to make this possible? Thanks. Regards Billy
Hello @BPart.1 ,
Better to ask that question in CubeMx forum board and link to that thread and close that one by accepting my answer above..
Internal ticket opened for CubeMx follow-up: 222721
2026-05-13 9:20 AM
@BPart.1 wrote:CubeMX does not allow me to configure this pin. Should this be hand coded to make this possible?
Indeed, it seems that this is a limitation of CubeMX - see:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.