2014-02-25 4:38 PM
I was able to download and install the STM32CubeMX plugin from ST (stsw-stm32095.zip) into my Eclipse 64-bit Kepler SR-1 software on a Linux 64-bit machine. Opening the perspective created a problem - An internal error of ''../plugins/com.st.microxplorer.rcp_4.0.0.201402191421//db/plugins/projectmanager/linux/64/toolgen.so not found'' message came up. Looking through the jar files in the zip file, it appears that only Windows dlls (32 and 64) can be found in the projectmanager directory of the plugin.
The slightly older version of microxplorer (pre-STM32CubeMX) dated from Sept 2013 was able to run, in it's own limited way, without hitting this type of error. Was Linux just overlooked with this plugin, or is it really just for Windows only? #bug #stm32cubemx #stm32cubemx-eclipse-linux2014-02-26 11:00 PM
Today the standalone version and the Eclipse plugin is supported on Windows only.
Due to this DLL not ported yet on MacOS or Linux it actually doesn't work. We should be able to address this issue in future versions Regards Daniel2014-03-04 10:58 AM
One additional point, if you just ignore this message you'll be able to perform all the functions of STM32CubeMX, including the code generation but no project files for IDEs will be generated.
Regards Daniel2014-03-22 3:16 AM
2014-03-26 11:43 PM
I agree. It's a shame that a company like ST released a non cross-platform plugin for an IDE whose main feature is being cross-platform.
2014-03-29 7:04 PM
You claim you can ignore this error? Nope, just a beautiful white window is present.
Linux is becoming a developers haven. I personally believe that hardware providers that are going to provide software and tools need to take this into serious consideration.Love the idea of the code generator, but not happy with the incompatibility.2014-04-17 3:54 AM
2014-08-04 3:16 PM
thanks JS for the info,
I have tried to install STM32CubeMX under WINE, everything worked great except the window for clock configuration showed nothing. am I the only one with this problem? any solution to this? OS: Linux Mint 17 WINE v 1.6.2 JRE-7u67-windows-i586 also installed in WINE2014-08-12 8:27 AM
Hello,
I have the same problem. The STM32CubeMX stand alone version works fine in wine exept the clock configuration, which is a major issue. Is there any kind of bugtracker? Sincerely Markus2014-08-28 6:00 AM
so why you write this software on java write it on pascal if you dont know what is java virtual machine lol!!! but if serious is a shame for ST or Microsoft pay for ST for discrimination Linux system or this software writen by windows Lusers!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.