2018-02-16 1:35 PM
I just upgraded to CubeMx 4.24 and attempted to migrate a STM32F7 project .ioc file. The migration failed with a Java null pointer exception when it reached the CAN IP portion.
To verify my .ioc file was not the culprit, I created a new project and the issue persisted. Here are the steps to reproduce:
Here is the topmost portion of the stack trace when it throws the exception:
2018-02-16 16:29:02,320 [INFO] UtilMem:68 - End LoadConfig() Used Memory: 2695795904 Bytes (3036151808)
2018-02-16 16:29:02,386 [INFO] ThirdPartyDb:293 - Open Third Party DataBase File (/home/david/.stm32cubemx/plugins/thirdparty/db/thirdparties_db.xml) : 0 ms. number of Sw pack : 0
2018-02-16 16:29:02,705 [INFO] PinOutPanel:995 - setPackage(No Configuration,No Configuration)
2018-02-16 16:29:02,706 [INFO] PinOutPanel:995 - setPackage(STM32F745VETx,LQFP100)
Exception in thread 'AWT-EventQueue-0' java.lang.NullPointerException
at com.st.microxplorer.plugins.ip.can.gui.CanManager.verifyValuePrescaler(CanManager.java:467)
at com.st.microxplorer.plugins.ip.can.gui.CanManager.clockChange(CanManager.java:72)
at com.st.microxplorer.plugins.ip.can.gui.CanManager.<init>(CanManager.java:59)
at com.st.microxplorer.plugins.ip.can.Can.onEnable(Can.java:53)
at com.st.microxplorer.plugins.ipmanager.pluginmanagement.IPUIPlugin.onEnablePlugin(IPUIPlugin.java:256)
at com.st.microxplorer.plugins.ipmanager.gui.BlockDiagram.enableDisableButtons(BlockDiagram.java:1065)
at com.st.microxplorer.plugins.ipmanager.gui.BlockDiagram.createPanels(BlockDiagram.java:439)
at com.st.microxplorer.plugins.ipmanager.gui.BlockDiagram.propertyChange(BlockDiagram.java:974)
at java.beans.PropertyChangeSupport.fire(PropertyChangeSupport.java:335)
at java.beans.PropertyChangeSupport.firePropertyChange(PropertyChangeSupport.java:327)
at java.beans.PropertyChangeSupport.firePropertyChange(PropertyChangeSupport.java:263)
at com.st.microxplorer.util.MXPropertyChangeSupport.firePropertyChange(MXPropertyChangeSupport.java:40)
at com.st.microxplorer.mxsystem.MxSystem.completeLoadConfig(MxSystem.java:369)
I have tried rebooting, removing and reinstalling CubeMx 4.24, and creating new projects from scratch. With this MCU, as soon as both CAN and ETH IPs are activated, I get this crash.
If it is possible to download CubeMx 4.23.0, please advise where I can do so. I need to get back up and running as soon as possible, as I have multiple active projects that depend on CubeMx heavily. It was working great up until now...
Thanks,
Dave#cubemx-4.24 #stm32cubemxSolved! Go to Solution.
2018-02-22 7:38 AM
Thank you
Rea.David
for all your comments.This issue will be fixed in the next CubeMX release.
Sorry for any inconvenience it may cause.
BR. Jeanne
2018-02-18 1:29 AM
Hello
Rea.David
,This issue is raised internally to CubeMX team.
You find old CubeMxversion in this discussion
https://community.st.com/0D50X00009XkYVDSA3
Best Regards,
Imen
2018-02-19 5:35 AM
Thank you
DAHMEN.IMEN
! I found a workaround that may help with resolution:The error appeared to be related to the prescaler check step when loading the CAN IP configuration block. It also occurred when clicking the 'CAN' button on the Configuration tab, before closing CubeMx in Step 6 above, but the application remained responsive.
Increasing the APB1 clock prescaler value to reduce the APB1 clock to 25MHz allows the IP to load successfully again. After this change, CubeMx can be closed and the project successfully re-opened. Setting the prescaler so that APB1 is clocked at 50MHz re-introduces the null pointer exception behavior.
So, the main issue seems unrelated to having the ETH IP loaded; rather it is because of the auto clock reconfiguration that occurs when adding the ETH IP to the project, which configures the APB1 bus.
Thanks,
Dave2018-02-22 7:38 AM
Thank you
Rea.David
for all your comments.This issue will be fixed in the next CubeMX release.
Sorry for any inconvenience it may cause.
BR. Jeanne
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.