2020-08-23 5:00 AM
Time to time cubeMX configurator includes c files in multiples, which I can clear by deleting one of them. But cubeMX insists adding multiples again in each regeneration. In freshly generated projects it doesn't do so. That issue appears only when I attempt to make a revision using the cubeMX configurator.
I am using cube IDE version 1.4.2 and :
cube MX
Version: 6.0.1-RC3
Build: 20200810-1643 (UTC)
In the attached image you can see multiple includes of system_STM32F1xx.c file. Project builds smoothly when I delete one of them.
2022-02-23 6:37 PM
yes this problem is so annoying .what can i do is creating a new project, It's a waste of time�?�?
2024-04-14 3:39 AM
I am having the same problem too. Is there any solution yet? I generate code each time this problem surfaces, to delete the extra files.
Thanks in advance
2024-10-18 1:31 AM
Hi all,
appends also with recent IDE versions, is not a solution but works
"Exclude from build" the template file
2024-10-18 1:35 AM
@Dimitris_Kara wrote:I am having the same problem too. Is there any solution yet?
I don't and, it seems, most users don't - so there must be something "odd" that you're doing.
Perhaps provide a complete & detailed description of the exact steps you take to get into this situation.
@Dimitris_Kara wrote:I generate code each time this problem surfaces, to delete the extra files.
What "extra files" ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.