2025-12-19 12:07 AM - edited 2025-12-19 12:21 AM
Hello.
It's not possible to find a controller with a specific number of CAN buses using MCUFinder.
MCUFinder counts each CAN bus twice:
If it physically has 3 CAN buses, MCUFinder adds:
3 CAN buses + the same 3 CAN2.0 buses = 6 CAN buses.
This is great if it allows the controller's peripherals to be doubled so easily. Excellent.
But it is very misleading because it raises false hope and displays completely unsuitable controllers.
However, the program is useless when I'm searching for controllers with 4 or more CAN buses and I get a huge list of 70 possible controllers, all of which have at least 6 CAN buses, but none of them possess these qualities.
Can this bug be fixed?
2025-12-19 12:40 AM - edited 2025-12-19 1:47 AM
Hello @Heinz_Baumer
Thanks for your valuable contribution.
A ticket 224139 has been escalated to dev team for further investigation.
I will keep you posted with updates.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.