2023-08-24 1:37 AM
Hello,
I have a problem trying to create a project in STM32CubeMX with a custom board using STM32L476RGT6 with crystal oscillator of 32MHz. In the interface configuration, when I selected HSE and set the value of 32MHz, it failed to initialize the peripherals because it got caught in a loop error by the clock configuration of the system. I have also verified the crystal signal and it corresponds to the frequency and if i select other options like HSI, everything works fine.
Looking for your advice to solve this problem,
Best regards,
2023-08-24 3:41 AM
Hello @User2501
First, I want to thank you for posting.
I tried the STM32 project which you described using the STM32CubeMX 6.9.1 version and I had 0 warnings and 0 errors.
I advise you to reproduce your project with the last version and I will be waiting for your feedback.
Thx.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-24 3:49 AM
> it got caught in a loop error by the clock configuration of the system
What does that exactly mean? What loop? What causes it? Single-step through the clock setup routine to find out - Cube is open source so you can do that.
> crystal oscillator of 32MHz
Is it a *crystal* or a *crystal oscillator*? Which model? If the latter, do you set RCC_CR.HSEBYP?
JW
2023-08-24 5:52 AM
Perhaps there's an issue with your hardware. Perhaps incorrect values on load capacitors. Can you share the schematic?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.