2018-11-05 2:09 PM
I have an IAR example STM32F746 project which brings up an LwIP stack on top of FreeRTOS; however I'm trying to turn it into a library and link into around 10-15 applications. This is breaking badly because linking via libraries doesn't appear to obey the __weak attribute.
The STM32F7xx_HAL_Driver uses __weak to expose symbols it allows the user to override, e.g:
__weak void HAL_MspInit(void)
I have an override of this in my application code (the auto-generated stm32f7xx_hal_msp.c file). When compiled as an application, the linker selects my version over the __weak version. When compiled as a library and then linked into an empty application, the linker selects the __weak version.
The only workaround I have found is to comment out the __weak versions of the functions when they have been overridden and my program works again.
Do you have any better suggestions than commenting out chunks of the HAL_Driver library?
---- UPDATE ---
I found a different solution which I believe works better than the current __weak approach. The __weak actually has two meanings:
The HAL_Driver library is attempting to use __weak in its first meaning where the user provided function overrides the default implementation. Instead the second approach works better. For example the declaration of HAL_MspInit should be:
__weak void HAL_MspInit(void);
Then its call in HAL_Init() should be replaced with:
/* Init the low level hardware */
if (HAL_MspInit)
HAL_MspInit();
Not only does this approach work for libraries, but this has the potential to be more efficient than the current approach in that the compiler has a chance of totally optimizing the call out for functions not implemented by the user.
There are something like 270 __weak functions in the STM32F7xx HAL_Driver library, and some of them actually do work if not overridden by the user (they need an else to the if in the example above). Food for thought!
2020-04-30 4:06 PM
I know this answer is much too late...
The usual cause of this in my experience, is due to the linker discarding the stm32xxxx_hal_msp.c file completely as there are no direct calls into that file. It thinks nothing calls those functions so they are unused. For example if you added a function into the stm32xxxx_hal_msp.c file and called it from another file, then the stm32xxxx_hal_msp.c file will not be discarded during linking and the weak functions will be overridden by the ones in stm32xxxx_hal_msp.c.
There are linker flags to prevent discarding unused sections, but they cause it to keep ALL unused sections.
This applies for sure with GCC but I don't know about IAR.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.