2019-03-19 4:17 AM
Hello,
The problem below has been solved.
There is no problem with the attached source code and the individual environment.
The problem was the board itself that I had.
Thank you for your interest.
Best regards.
Song
===========================================================================
Hello.
I have a problem initializing CAN communication through the HAL library on STM32CubeMX, so I'd like to ask you about a related issue.
First of all, the development environment that I use is:
- MCU: STM32L443CCT6
- Computer: IAR EW ARM 8.32.1.18631
- Initialize CAN communication: 500 Kpbs
- Code generation tool: STM32CubeMX (HAL STM32Cube FW_L4 V1.13.0)
I have already successfully initialized CAN communication on the STM32F303CC chip without difficulty and data transmission in the same development environment as above.
Based on the above successful example, I generated an initialization code for CAN communication on the STM32L443CCT6 chip currently being developed.
This generated code is a simple code with CAN communication initialization and data transfer only.
However, unlike the previous experience shown on the STM32F303CC chip, CAN communication initialization and data transfer is not possible.
Circuits have the same configuration, only chips are different. Please help and support me if the code I created is missing or problematic.
For your information, we are attaching the relevant code.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.