2024-07-02 8:03 AM - last edited on 2024-07-02 10:30 AM by Tesla DeLorean
Hello,
I think I might have found a bug source in the CubeMX's generated code, when two components of a same driver share the same clock.
Here I'll use the example of the ADC 1 and 2 of the STM32H743GTV6 but I have see this case a few times elsewhere.
As the two ADC use the same clock, to avoid initiating it while the other is already using it, a check variable is used:
static uint32_t HAL_RCC_ADC12_CLK_ENABLED=0;
void HAL_ADC_MspInit(ADC_HandleTypeDef* adcHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(adcHandle->Instance==ADC1)
{
/* USER CODE BEGIN ADC1_MspInit 0 */
/* USER CODE END ADC1_MspInit 0 */
/* ADC1 clock enable */
HAL_RCC_ADC12_CLK_ENABLED++;
if(HAL_RCC_ADC12_CLK_ENABLED==1){
__HAL_RCC_ADC12_CLK_ENABLE();
}
/* Some code */
}
else if(adcHandle->Instance==ADC2)
{
/* USER CODE BEGIN ADC2_MspInit 0 */
/* USER CODE END ADC2_MspInit 0 */
/* ADC2 clock enable */
HAL_RCC_ADC12_CLK_ENABLED++;
if(HAL_RCC_ADC12_CLK_ENABLED==1){
__HAL_RCC_ADC12_CLK_ENABLE();
}
/* Rest of the function */
}
}
And the same thing is done is the void HAL_ADC_MspDeInit(ADC_HandleTypeDef* adcHandle) function:
HAL_RCC_ADC12_CLK_ENABLED--;
if(HAL_RCC_ADC12_CLK_ENABLED==0){
__HAL_RCC_ADC12_CLK_DISABLE();
}
But in the case where HAL_ADC_MspDeInit is called before HAL_ADC_MspInit, the HAL_RCC_ADC12_CLK_ENABLED (initiated to 0) will be 0xFFFF FFFF and so the init won't work.
I think something like that would be enough:
if(HAL_RCC_ADC12_CLK_ENABLED!=0){
HAL_RCC_ADC12_CLK_ENABLED--;
if(HAL_RCC_ADC12_CLK_ENABLED==0){
__HAL_RCC_ADC12_CLK_DISABLE();
}
}
Best regards,
Sulian
Solved! Go to Solution.
2024-07-02 10:16 AM
Yes this is a known issue but a more complicated solution would be er... more complicated. So in the end, the developer is responsible to find a satisfying solution.
2024-07-02 10:16 AM
Yes this is a known issue but a more complicated solution would be er... more complicated. So in the end, the developer is responsible to find a satisfying solution.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.