2021-09-28 12:47 AM
Hello!
I am working on STM32 (H7) project , when I click OC file it creates STM32CubeMX and it develop a dialogue which ask, with the help of STM32Cube firmware FW_H7 V1.9.0 this project was designed. With the usage of STM32Cube firmware version FW_H7 V1.9.0. the function of new STM32Cube V6.3.0 is better.
I have a confusion I am at V1.9.0, already , but in case if I choose <Migrate> then make Cube MX return back with <Generate Code>.With the redesigning of project the floating point variables ‘ output no more working.
Instead of Migrate if I choose continue Cube MX shows an empty screen
STM32CubeIDE is v1.7.0
I want suggestions regarding this problem.
Thank You.
2021-09-28 1:46 AM
Hello @Enora.1 !
Can you please provide me with your IOC file ?
Thank you,
Mouadh.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.