2023-12-13 3:05 AM
When I generate code for the MPU region 0 wit HAL I get:
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
MPU_Attributes_InitTypeDef MPU_AttributesInit = {0};
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x08fff800;
MPU_InitStruct.LimitAddress = 0x08fff900;
MPU_InitStruct.AttributesIndex = MPU_ATTRIBUTES_NUMBER0;
MPU_InitStruct.AccessPermission = MPU_REGION_ALL_RO;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_OUTER_SHAREABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
MPU_AttributesInit.Number = MPU_REGION_NUMBER0;
MPU_AttributesInit.Attributes = MPU_DEVICE_nGnRnE | MPU_WRITE_THROUGH
| MPU_TRANSIENT | MPU_NO_ALLOCATE;
HAL_MPU_ConfigMemoryAttributes(&MPU_AttributesInit);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}OK.
With the exact same configuration, when I switch to LL I get:
void MPU_Config(void)
{
/* Disables the MPU */
LL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER0, LL_MPU_INSTRUCTION_ACCESS_DISABLE, LL_MPU_ATTRIBUTES_NUMBER0, 0x08fff800, 0x08fff900);
LL_MPU_EnableRegion(LL_MPU_REGION_NUMBER0);
LL_MPU_ConfigAttributes(LL_MPU_ATTRIBUTES_NUMBER0, LL_MPU_DEVICE_nGnRnE | LL_MPU_WRITE_THROUGH
| LL_MPU_TRANSIENT | LL_MPU_NO_ALLOCATE);
/* Enables the MPU */
LL_MPU_Enable(LL_MPU_CTRL_PRIVILEGED_DEFAULT);
}I think there are not equivalent. There is a missing :
| LL_MPU_REGION_ALL_RO | LL_MPU_ACCESS_OUTER_SHAREABLEin the 2nd parameter of LL_MPU_ConfigRegion().
Is this true?
Solved! Go to Solution.
2023-12-18 9:16 AM
Hello @Nikita91
First let me thank you for posting.
In fact you are right, I made the test adding the missing code, and only then I get the same MPU registers configuration done by the HAL generated code.
The issue is raised internally for analysis and future fix (169120: this is an internal ticket number)
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-18 9:16 AM
Hello @Nikita91
First let me thank you for posting.
In fact you are right, I made the test adding the missing code, and only then I get the same MPU registers configuration done by the HAL generated code.
The issue is raised internally for analysis and future fix (169120: this is an internal ticket number)
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.