2022-09-27 5:43 AM
In the manual RM0468 for the STM32H730 say that the reg "PWR_D3CR" bits "VOS" has
00: Scale 0
01: Scale 3 (default)
10: Scale 2
11: Scale 1
Also in the code defines in "stm32h7xx_hal_pwr.h"
#define PWR_REGULATOR_VOLTAGE_SCALE0 (0U)
#define PWR_REGULATOR_VOLTAGE_SCALE1 (PWR_D3CR_VOS_1 | PWR_D3CR_VOS_0)
#define PWR_REGULATOR_VOLTAGE_SCALE2 (PWR_D3CR_VOS_1)
#define PWR_REGULATOR_VOLTAGE_SCALE3 (PWR_D3CR_VOS_0)
But in CubeMX Version "6.6.1" Lib version "1.10.0"
Only Scale 0,1,2 is selectebel. Se image
Solved! Go to Solution.
2022-09-27 6:40 AM
Hello @MRick.2,
To enable VOS3 on an STM32H730, the core frequency Fcpu must be at most 170 MHz. I suppose that in your STM32CubeMX project, the core frequency is in the interval ]170MHz, 300MHz].
For further details, I suggest you refer to DS13315 page 108.
I hope you find this helpful !
Aziz
2022-09-27 6:40 AM
Hello @MRick.2,
To enable VOS3 on an STM32H730, the core frequency Fcpu must be at most 170 MHz. I suppose that in your STM32CubeMX project, the core frequency is in the interval ]170MHz, 300MHz].
For further details, I suggest you refer to DS13315 page 108.
I hope you find this helpful !
Aziz
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.