2023-10-12 12:07 AM
Because I don't want use HAL , but want use the possibility to configure pins with CubeMX
Solved! Go to Solution.
2023-10-12 1:18 AM
Hello @sven ,
STM32CubeMX supports custom code generation by means of a FreeMarker template. Check the UM1718 section 6.3 Custom code generation.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-12 12:22 AM
on many peripherals you can choose also LL (low level ) lib , or HAL.
+
you can also use cube/HAL or LL just to do init (as i do sometimes) and then in program write direct to registers for max. speed. (if possible...no good idea for USB communication, for example)
2023-10-12 1:18 AM
Hello @sven ,
STM32CubeMX supports custom code generation by means of a FreeMarker template. Check the UM1718 section 6.3 Custom code generation.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.