2023-10-12 2:15 AM
Hi,
I cannot enable SPI1 interface in CubeMX with STM32F427.
I only see the message "I2S1" must be disabled":
But I2S is not used in my project.
In Pinout view it is possible to select Pins PA4 to PA5 and PB5 for SPI1-sugnals without error messages.
Whats wrong here?
Solved! Go to Solution.
2023-10-12 2:57 AM
I tried a complete new empty project, and it was the same: SPI1 was greyed out.
Then I closed CubeMX and started it as administrator: and it works :thinking_face:
No idea, what is the difference, but I can go on now with my project.
2023-10-12 2:54 AM
Hello @ReinhardD
Can you share your .ioc file if possible to reproduce your issue and which CubeMX version do you use?
Thank you
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-10-12 2:57 AM
I tried a complete new empty project, and it was the same: SPI1 was greyed out.
Then I closed CubeMX and started it as administrator: and it works :thinking_face:
No idea, what is the difference, but I can go on now with my project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.